AnsweredAssumed Answered

migrating from VDSP++ to CCES

Question asked by bookevg on Sep 24, 2012
Latest reply on Oct 31, 2012 by CraigG

I trend to locate source files outside from VDSP++ project directory.

I located source files outside from VDSP++ project directory using relative commnad like ..\..\

I find that I can change PROJECT_LOC or PARENT_LOC using Select Path Variable, but I work in team and the absolute adrress don't be satisfied me.

How can I do it like it was in VDSP++?

For example:

Projects.AD

     -VDSP++

     -CCES

          -.metadata

         -MCS - There are located CCES project files

     -Source  - There are located CCES source files

           -Library

           -Projects

                -MCS

I tried to create the new folder: Link to alternate location (Linked Folder)

PROJECT_LOC/../../Source

(PROJECT_LOC = Projects.AD\CCES\MCS)

and I got

Internal error: Must specify a URI scheme:Source

I solved the problem: I created a new location path:

OUTSIDE_LOC = the path of Projects.AD

and

now when I create linked pathes I use OUTSIDE_LOC, but I want to use PROJECT_LOC or WORKSPACE_LOC

Outcomes