AnsweredAssumed Answered

Single Phase Power Measurement on per cycle basis

Question asked by jerryw on Sep 19, 2012
Latest reply on Sep 27, 2012 by hmani

I need single phase power measurements of 60 and 50 hz power with power calculated cycle by cycle. The current input is from a CT 1mA/A and the voltage input is from an isolation amplifier. the power range is .25 KW to 25 KW. I need outputs proportional to RMS Volts and RBS Current.

 

What device is best suited to this application?

Outcomes