AnsweredAssumed Answered

ADV7511W as a DVI transmitter with YCbCR input and RGB output

Question asked by hasenmi on Sep 18, 2012
Latest reply on Sep 27, 2012 by GuenterL

I must be dense; I do not seem to understand the minimum register settings to use the ADV7511W as a simple DVI transmitter with YCbCr 4:2:2 input and RGB output.

 

I can't even get the device to send usable syncs to a receiver.

 

Is there a set of 'reference' files that have a know setup programmed into the ADV7511W that will be able to be recognized by DVI receiver?

 

In other words... I need help, and I am willing to beg (Since I have so little hair left).

 

My need is 1024x768 @ 60Hz.

 

Thanks, for any help, in advance.

 

Mike

Outcomes