AnsweredAssumed Answered

Possible inaccuracy in STEP model for ADIS16488?

Question asked by miguelp on Sep 18, 2012
Latest reply on Sep 28, 2012 by NevadaMark

I'm trying to determine where to place the mating connector for the ADIS16488.  Based on the dimensions in the datasheet (p.33), it seems that the mid-line of the connector should be 1.642mm from the mounting hole.  However, this connector placement does not quite line up with the connector in the ADIS16488 step model I downloaded from Analog Devices. 

 

I'm inclined to go with the datasheet dimensions, but it would be great if somebody could confirm this error in the step model so I know I'm not somehow reading the dimensions wrong.

 

Thanks!

Outcomes