AnsweredAssumed Answered

AD9914 PARALLEL PROGRAMMING

Question asked by serdar on Sep 13, 2012
Latest reply on Sep 13, 2012 by DSB

Hi,

 

I want to use the AD9914 in the parallel programming mode, thus set F(3-0) to “0000”. I plan to use 16 bit data width so the parallel data port shall be used as follows:

DataPort(31-16) -> Data(15-0)

DataPort(15-8)   -> Address(7-0)

DataPort(0) -> “1” (indicating 16 bit operation)

DataPort(1) -> RDB

DataPort(2) -> WRB

 

All seems to be clear up to here but when the IO_UPDATE pin come into play my mind confuses. IO_UPDATE pin is not referenced throughout the parallel programming section. Never mentioned about it within the timing waveform. I suppose that the signals named as RD and WR in the timing diagrams is the RDB and WRB respectively. I conclude that it is possible to set the IO_UPDATE pin to constant “1” and use the entire DataPort(31-0) as a transparent port. Then this port becomes a regular read/write port with the data, address and regular strobe signals. I want to be sure if this kind of usage is permitted or do I have to toggle the RDB/WRB bits with successive writes to that port in which IO_UPDATE is the write strobe.

 

Thanks

Serdar

Outcomes