AnsweredAssumed Answered

Any issue on the SPI feature of the ADUC7020 in slave mode?

Question asked by DSPDSP on Sep 12, 2012
Latest reply on Sep 18, 2012 by PatrickN

Hello,

 

I am using the ADUC7020 in spi slave mode withtout interrupt.

Just by checking the register SPISTA for the RX and TX .

I am using 8 bytes packets with clock phase =1 and clock polarity =1.

The master provides clock patterns based on 8 falling edges and 8 rising edges.

KNowing that if i expect a answer of n bytes, i have to provide the TX register with one command + dummy data in order to provide the clock, i observe very erratic data on the RX register.

 

Is there any advice or known tricks about the SPI management for this target?

 

 

Regards

Thank you

Outcomes