AnsweredAssumed Answered

RF input driver to the Mixer

Question asked by veera on Sep 10, 2012
Latest reply on Sep 10, 2012 by Qui

In the Data sheet of the Differential Amplifier AD8352, it is mentioned that it can be used as Mixer driver.

Can you share us any application circuit where this is used as Mixer driver?

Is it sufficient that we connect the output of the AD8352 to any 50 ohm input Mixer through 1:3 Transformer, or should we need to do additional circuitry?

Outcomes