AnsweredAssumed Answered

SPI Slave booting using software solution

Question asked by SMAM on Jul 6, 2009
Latest reply on Jul 24, 2009 by Matt

 

 

Hi,

 

    I am using the SPI slave booting for bootloading the ADSP21369 using a microcontroller, where the ADSP21369 is the slave and microcontroller is a master. I am using the Software solution given in EE-177 (SHARC SPI slave booting). The SPI baud rate is 625 KHz

 

I am using the software solution based on EE-177 to pause the bootloading when the ADSP21369 is initialising the zero-init sections.

 

Can anyone please answer my questions below:

 

1)      Is the FINAL_INIT section the last section? Can there be any other sections after the Final init.

 

2)      How do we find the word count of the FINAL_INIT section.

 

3)      If I am using single processor, will there be a MULTI_PROC section?

 

4)      Should we initialise the core speed and SDRAM in the kernel or in the application code? What difference does it make?

 

Thanks very much.

 

                Regards,

                SM

Outcomes