AnsweredAssumed Answered

ADSP21364 - SRU

Question asked by savinat on Jul 6, 2009
Latest reply on Jul 9, 2009 by savinat

Hi,

I am using SPIB on ADSP21364 but having problems with connecting  the SPIB signals to DAI pins. The SPI is in master mode and the CCLK is output and i connected it on DAI pin 10. Does it have to be this pin configured as an  output?For example:

 

SRU (HIGH, PBEN10_I);
SRU (SPIB_CLK_O, DAI_PB10_I);

 

Is that true? And how can i chek if  this signal  is realy  conecting to DAI pin 10?

 

I allso did that: 

SRU (HIGH, PBEN11_I);

SRU (SPIB_MOSI_O, DAI_PB11_I);

 

SRU (LOW, PBEN12_I);
SRU (DAI_PB12_O, SPIB_MISO_I);

Is it true tha too?

Outcomes