AnsweredAssumed Answered

AD7760 - /DRDY pulse width

Question asked by Mr.K on Aug 31, 2012
Latest reply on Sep 24, 2012 by MClifford

Hi,

I have a question about /DRDY of AD7760.

 

My device setting is as follows.

 

・Filterd Output

MCLK = 40MHz

Control Register 2 = 0x0092

     : /CDIV = 0 (ICLK = 1/2 MCLK = 20MHz)

Control Register 1 = 0x001A

 

In the data sheet, the pulse width of /DRDY is "0.5 × tICLK".

However, the /DRDY pulse width of my circuit is "tICLK(50ns)".

 

Is this behavior correct though the /DRDY pulse width of my circuit is different from the data sheet description?

 

Regards,

Mr.K

Outcomes