AnsweredAssumed Answered

ADSP21364 - SPI

Question asked by savinat on Jul 4, 2009
Latest reply on Jul 7, 2009 by Mitesh

Hi to all !!

I am connectin ADSP21364 to codecADAU1361 over SPORT and SPI. The CCLK on the codec is max 10MHz. And the SPI on DSP is in master mode so the CCLK of the codec is provided from the DSP. How can i set the clock of SPI for this value with the SPBAUD - what should be the value in SPIBAUD to provide 10MHz or less?

And i have another problem. It turns ou that the SPI signals of ADSP aren`t  move in extarnal bus. So can i rout them with SRU to DAI pins?

Outcomes