AnsweredAssumed Answered

Could AD-FMCOMMS1-EBZ be modified to receive/transmit up to 6 GHz?

Question asked by skao@nmi on Aug 27, 2012
Latest reply on Sep 4, 2012 by skao@nmi

Hi,

 

We're very interested in purchasing this module, the only one major limitation for our purposes is the maximum RF receive/transmit frequency. Could the board be modified to be able to receive and transmit up to 6 GHz? From the block diagram, it appears that the modulator/demodulator are already capable. It seems like the only part(s) that would need to be swapped are the ADF4351 synthesizers and the ADL5602 amplifier. Are there other AD part that would fit perfectly in their place that could go up to 6 GHz? We do not need to go any lower than 2 GHz.

 

If possible, we would like to work with AD engineers to ensure the quality of the design.

 

Thanks so much,

Sean Kao

Outcomes