AnsweredAssumed Answered

ADF4360-8 as variable Local oscillator

Question asked by SAURABH on Aug 25, 2012
Latest reply on Aug 27, 2012 by rbrennan

i want to use ADF4360-8 as local oscillator that can be used in 65-400 MHz simultaneously. in data sheet it is written that Center frequency is set by external inductors,does it mean for 65 MHz output and 400 MHz output i have to change the inductors.

 

                            if  i want to use LO source  51.4 MHz to 442 MHz then  which PLL i have to opt.

Outcomes