AnsweredAssumed Answered

AD9912 power supply

Question asked by SAURABH on Aug 25, 2012
Latest reply on Aug 27, 2012 by LucaV

i am using AD9912 as a LO source for battery operated equipment. for that one i am desining power supply section( input volatge from battery is 14.8Volt )

 

1) 14.8 V to 5V  through Switching regulator (part No RECOM regulator)         then LDO  AD3338               for 3.3 Volt

2)  14.8V to 2.2 V through Switching regulator(part no yet not finalized, LMZ1002 from TI)         then LDO ADP172                for 1.8 Volt (300mA Load)

how much  PSRR and ripple will be achieved with ADP172 (because drop out volatge is less than 1 Volt)

or we can decrase the input to ADP172 to increase the efficiency  insipte PSRR & Ripple will not reduced .

   two switching regulator in one board will not create any problem ( because board contain RF circuits.)  or i have go to  any other approch.

Outcomes