abdullah

fwrite/ fputc error

Discussion created by abdullah on Jul 2, 2009
Latest reply on Feb 16, 2010 by jobo23
I am using BF537 ez kit lite.
I am implementing its example  .............\Analog Devices\VisualDSP 5.0\Blackfin\Examples\ADSP-BF537 EZ-Kit Lite\Getting Started Examples\Part_2_1.
Simply i have defined a File pointer in it and read a file and store it in a dynamically created chracter array. Its ok.
The problem is when i save this file to the disk using fwrite, it writes the file but after some interval 4 bytes are re copied as shown in figure attached. Why these bytes are re-copied. If you save it at once or in chunks same problem occours.
I have checked the data of array its ok but i dont no why its is not writing the whole array truely into the file.
Figure:-
Two files are compared (actual file and saved file) which are in background.
Result of comparasion is in the file which is on forefront.

Attachments

Outcomes