AnsweredAssumed Answered

confusion about 7612's HDMI automatic CSC

Question asked by rqiu@qualcomm.com on Aug 21, 2012
Latest reply on Aug 28, 2012 by BrianE

Page 107 of the doc UG-216 says "In HDMI mode, the ADV76122 provides an automatic CSC function based on the AVI InfoFrame sent from the source".

 

How should I set INPUT_COLOR_SPACE and RGB_OUT to enable this feature?

 

Another question is about OP_656_RANGE_SEL: If the range of source is limited to 16:235, and OP_656_RANGE_SEL is set to 0, will the CSC be enabled (assuming the color space of input and output are set to the same)?

 

Thank you.

Outcomes