AnsweredAssumed Answered

How to connect an ADuC7024 to an Xbee radio

Question asked by TiagoR on Aug 20, 2012
Latest reply on Aug 21, 2012 by TiagoR

I'm trying to understand how I can connect (hardware)  the ADuC7024 on a Xbee. I need to know what pins: TX, RX, GND, VDD(3.3V) are available in the ADuC7024 to connect in the Xbee. You can see below an tutorial explain how you can connect an Arduino to an Xbee. I think the pin J3-1 (AVDD) it's already 3.3 V so I can connect in the VCC(3.3V) Xbee's Pin, that's right? But TX and RX I'm not sure. I think that I need to used GPIO pins. I think it will be something like:

 

GP1CON = 0x11 // Setup TX and RX pins on P1.0(Receive Data) and P1.1 (Transmit Data)

 

Tutorial: http://answers.oreilly.com/topic/2458-how-to-connect-an-arduino-to-an-xbee-radio/

 

I just want a help. Is is configured correctly?

 

Thank you very much!!

Outcomes