AnsweredAssumed Answered

AD9547, AD9548, AD9549 EV-Boards

Question asked by Fred1 on Aug 16, 2012
Latest reply on Aug 16, 2012 by pkern

Hi,

 

I have a few questions regarding the AD954x Evaluation boards.

 

1. Can the AD9548 EV-board be used to evaluate the performance of the AD9547 provided reference is >1kHz and I/O's are limited to the number available on the AD9547? (We do have a few AD9548 EV Boards)

 

2. What is from the performance point pf view the difference between the AD9547 and AD9549? We want to produce a stable output frequency of 200 MHz from a jittery 8kHz reference. We also need a "Self disciplining" functionality which is available on the AD9547/8. Adjusting the phase of the output signal is also required.

 

Regards,

Fred

Outcomes