AnsweredAssumed Answered

218x and IRQ1 interrupt not working

Question asked by sketkar on Jun 24, 2009
Latest reply on Jun 26, 2009 by StuartS

Hello,

 

I'm using the interrupt handler to setup IRQ1 interrupt as well as a timer interrupt

 

interrupt (SIGTIMER, timer_isr) seems to work fine but interrupt(SIGIRQ1, irq1_isr) crashes the application sent it to __exit, ___lib_prog_term, __Exit in the Disassembly everytime the interrupt occurs.

 

The IMASK is getting setup correctly and the ICNTL is set to edge trigger, which also correct.

Outcomes