AnsweredAssumed Answered

need help with enabling "Expert Linker" option on the project

Question asked by mazx on Aug 6, 2012
Latest reply on Aug 10, 2012 by CraigG

I'm having trouble with figuring out why "Tools->Expert Linker->Create LDF" is disabled (grayed out).

 

Some of the documentation on "Expert Linker" mentioned that this can happen if your target controller is not supported or you don't have a project open. In my case, my target controller is B537 and the project is open.

 

VDSP info: V5.0 Update 9.1

 

"Project Options -> General" tab details

Processor: ADSP-BF537

Revision: Automatic

Type: Loader File

 

"Project Options -> Add Startup Code/LDF" tab details

"Don't add an LDF or startup code" option is selected

 

Is there something obvious that I'm missing?

 

Thanks in advance

Outcomes