AnsweredAssumed Answered

Pitch Transposer - Range

Question asked by Bill.PE on Aug 2, 2012
Latest reply on Aug 29, 2012 by Bill.PE

I got to spend so more time with this module and I see some really strange things.  If you set the MAX RANGE to 100, send in a 1kHz tone and the slider from left to right outputs 700 to 1300 Hz.  This does not match the infomation in the Wiki.  The output is also amplitude modulated even with a constant amplitude input.  Changing the delay has not fixed that.  Any explanation for this?

Outcomes