AnsweredAssumed Answered

Enable Asterisk in Menuconfig

Question asked by nickabrham on Jul 30, 2012
Latest reply on Aug 3, 2012 by Aaronwu

Hi Everyone,

I have few queries related to enabling Asterisk according to the document http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:asterisk. These queries are as follows

  1. Does anyone ever successfully run Asterisk on BF-537 Stamp Board along with the PBX hardware - 2FXS+2FXO daughter card. I have developed my own PBX hardware - 2FXS+2FXO daughter card according to the schematic provided at the following link http://download.analog.com/27516/frsrelease/1/1/4/1142/2FXO_2FXS_card_sch.pdf.
  2. According to the document http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:asterisk, it is mentioned that one should use 2007R1 and 2006R2 releases of Blackfin Toolchain and uCLinux distribution. Can I use the latest toolchain along with the latest uCLinux distribution to create the final image with asterisk enabled?
  3. I am able to create the final image using http://blackfin.uclinux.org/gf/download/frsrelease/348/3283/blackfin-toolchain-07r1.1-3.i386.rpm 2007 release toolchain, the  http://blackfin.uclinux.org/gf/download/frsrelease/350/3340/uClinux-dist-2007R1.1-RC3.tar.bz2 uClinux distribution and then enable Asterisk according to the document http://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:asterisk.
  4. This created image easily loads onto the BF-537 Stamp Board through TFTP, but when I run the bootm command, following message is displayed "Verifying Checksum ... Bad Data CRC"
  5. Although creating only uClinux image without enabling asterisk does not give any errors.

Kindly provide answer to these asap.

 

Regards,

Nick.

Outcomes