AnsweredAssumed Answered

TFTP problem in uClinux 2011R1RC3

Question asked by karthikeyan on Jul 28, 2012
Latest reply on Jul 30, 2012 by karthikeyan

Hi,

    We are using the uClinux 2011R1RC3 version of the distor with the tftp folder updated to the changes mentioned in the http://ez.analog.com/thread/10915 thread. We are using toolchain 2011R1RC4 to compile the distro and create the image. I had earlier posted about the problem in tftp at the following thread http://ez.analog.com/thread/10915 and the issue was fixed for get file. At that time we did not check the put file functionality. Now we are experiencing a problem with the put file. Either we are doing something wrong or the put file is having problem some issues. Please find the following log message. Also it gives segmentation fault (SEGV) when enter is pressed without any commabd in the tftp prompt.

 

root:/> pwd

/

root:/> ls test.txt

test.txt

root:/> tftp 192.168.40.211

tftp> get touchScreen_example_static

Received 100462 bytes in 0.1 seconds

root:/> cp test.txt /root/

root:/> cp test.txt /home/

root:/> tftp 192.168.40.211

tftp> get touchScreen_example_static

Received 100462 bytes in 0.0 seconds

tftp> put test.txt

Error code 1: File not found

tftp>

SEGV

 

The following telemetry shows the SEGV fault thorwn when enter is pessed with no command at the tftp prompt


root:/> tftp 192.168.40.211

tftp>

SEGV

root:/>

Outcomes