AnsweredAssumed Answered

Single link mode output on AD9644

Question asked by r.traylor on Jul 27, 2012
Latest reply on Aug 1, 2012 by J.Harris

In single link mode, (referred to as the third output mode) both converters are output on

one link using two lanes and  only DSYNCA.  After conversion to 8b/10b and optional

scrambling, are the MSBs (bit19) of both converters output first, followed by the next

most MSB,and so on down to bit zero? 

 

This seems identical to the first mode, with the exception of one DSYNC being used

instead of two.  Is that right? 

 

Does ADI have a simulation model for the digital output part of the converter?

 

Thanks

Outcomes