AnsweredAssumed Answered

Memory overlay or multiple DXEs?

Question asked by microlab on Jul 24, 2012

Hi,

 

I'm developing a project that involves 2d barcode image processing and decoding using BF592. As the overall code size will be bigger than 32K bytes, so I am planning to split it into 2 parts, 1st parts does the image and data pre- /post-processing and the 2nd part just does the barcode decoding. My idea is when the system is powered up, the 1st part will be loaded in and process image/data, and then load in the 2nd part to decode the barcode, success or not, re-load in the 1st part to do the post-processing, and wait for the next image.

 

The code size of both parts will be bigger than 20K and each involves dozens of function calls, so  which one should I choose in my application, memory overlay or multiple DXEs?

 

Thanks,

microlab

Outcomes