AnsweredAssumed Answered

sdata_outx ADAU1701

Question asked by Vuagniav on Jul 18, 2012
Latest reply on Jul 19, 2012 by BrettG

Hi,

 

I'm trying to use the sdata_out pin of the ADAU1701 evaluation board.

I would send the signal from the ADC0 and ADC1 to the sdata_out0 with left-justified mode.

I would use the ADAU1701 as master so I connected the OUTPUT_LRCLK with the INPUT_LRCLK and the OUTPUT_BCLK with the INPUT_BCLK.

I configure the MP6 as SDATA_OUT0. Now my problem is that I don't know how to put the data from the ADC0 and ADC1 to the SDATA_OUT0...

 

Thanks for the help

Outcomes