AnsweredAssumed Answered

Question on AD9833

Question asked by haitaoli7036 on Jul 18, 2012
Latest reply on Jul 19, 2012 by haitaoli7036

Hi, I am using AD9833 to generate a sine wave whose frequency is from 0.1Hz to 10kHz, the amplitude is 20mV and DC offset is 2.5V. The output of AD9833 is from 38mV to 650mV. What should I do to change the DC offset and amplitude? Thanks!

Outcomes