AnsweredAssumed Answered

AD9963 DAC Common Mode Voltage

Question asked by arunashok on Jul 18, 2012
Latest reply on Jul 19, 2012 by arunashok

How can one set the output common mode voltage of the DAC of AD9963. The full scale current is (Ifs) 2 mA and does it implies the common mode voltage level is  Ifs/2 * R.   I need to interface the DAC to another module which has the common mode range of 1.5 V. Its written in the data sheet that with TXVDD 3.3 and TXCML 0.5 V the maximum common mode output level can be 1.25 V but its mentioned that the output compliance range for the same setting is 1.7V..  Why is that...

Outcomes