AnsweredAssumed Answered

ADuCM360 Quick Start Plus Development Kit

Question asked by mwiggins on Jul 6, 2012
Latest reply on Mar 1, 2018 by amcl

I have just received the ADuCM360 Quick Start Plus Development Kit and downloaded all the latest documentation and software as suggested from ftp://ftp.analog.com/pub/MicroConverter/ADuCM360V0.2/

 

After setting up the Keil IDE with the demo project as it describes in the ADuCM36x Getting Started Guide, I attempt to download the compiled program to the board.

 

At first I get this error

No Cortex-M SW Device Found

Error: Flash Download failed - Target DLL has been cancelled

 

Then, I pull the ADuCM360 Minikit board off the Interface board and replace it.  I then try the download again and I get this.

Could not stop Cortex-M device! Please check the JTAG cable.

Error: Flash Download failed - Target DLL has been cancelled

 

The Build Output window shows the following:

Load "C:\\ADuCM360V0.2\\Example Code\\RealView\\Programs\\ADIdemo\\Demo.AXF"

* JLink Info: Device "UNSPECIFIED" selected (0 KB flash, 0 KB RAM).

Set JLink Project File to "C:\ADuCM360V0.2\Example Code\RealView\Programs\ADIdemo\JLinkSettings.ini"

 

JLink info:

------------

DLL: V4.50k, compiled Jul  2 2012 16:03:19

Firmware: J-Link ARM Lite V8 compiled Jun 19 2012 14:36:11

Hardware: V8.00

S/N : 228200118

 

* JLink Info: Found SWD-DP with ID 0x2BA01477

* JLink Info: FPUnit: 6 code (BP) slots and 2 literal slots

* JLink Info: Found Cortex-M3 r2p0, Little endian.

ROMTableAddr = 0xE00FF003

* JLink Info: SYSRESETREQ has confused core. Trying to reconnect and use VECTRESET.

* JLink Info: Found SWD-DP with ID 0x2BA01477

**JLink Warning: Failed to reset CPU. VECTRESET has confused core.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

* JLink Info: Core did not halt after reset, trying to disable WDT.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

**JLink Warning: Could not set S_RESET_ST

* JLink Info: Found SWD-DP with ID 0x2BA01477

* JLink Info: SYSRESETREQ has confused core. Trying to reconnect and use VECTRESET.

* JLink Info: Found SWD-DP with ID 0x2BA01477

**JLink Warning: Failed to reset CPU. VECTRESET has confused core.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

* JLink Info: Core did not halt after reset, trying to disable WDT.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

**JLink Warning: Could not set S_RESET_ST

***JLink Error: Could not read flash patch control register.

* JLink Info: Device "UNSPECIFIED" selected (0 KB flash, 0 KB RAM).

**JLink Warning: CPU could not be halted

 

Any help is appreciated!

Outcomes