AnsweredAssumed Answered

AD7606 range pin behavior

Question asked by klarsen on Jul 2, 2012
Latest reply on Jul 10, 2012 by klarsen

I'm using the AD7606 eval board in standalone mode. I have installed R1 which pulls the range pin to logic high. This means +/-10V range. But I'm not seeing this range. It is behaving as if in the 5V range.

 

Is there anything else I need to do to ensure that I am actually operating in the 10V range?

 

As a side note, I'm operating in SPI mode.

Outcomes