AnsweredAssumed Answered

ADP2302 ADIsimPower

Question asked by zanzibar on Jun 29, 2012
Latest reply on Jul 9, 2012 by zanzibar

hi,

 

I try to use ADIsimPower with ADP230x buck designer v2.1 file.

 

I tried :

Vin min : 11V

Vin max : 15V

Vout : 5V

Iout : 2A

Ambient temp : 55°C

Design for : cost

 

I click on "view solution". There are some errors with L1 and C1 values but I did not succeed to change them.

 

Can you help ?   

Outcomes