AnsweredAssumed Answered

DC coupled VGA with single-ended in/out?

Question asked by jose.martin on Jun 29, 2012
Latest reply on Jul 2, 2012 by jose.martin

Hello,

 

I'm building a input stage for an ADC, the analog BW should be around DC to 100 Mhz.

I'm looking for a DC coupled VGA with single-ended input and output, The AD8337 seems to be a good candidate but i don't have the tools to use the LFCSP package,

AD8370 has TSSOP package and can be DC coupled (http://ez.analog.com/message/30236#30236), but it has differential output.

 

My question if there is an VGA which can be configured to DC coupled with single-ended output and TSSOP or similar package.

Single or dual power supplies aren't a problem (+5 or +5/-5 are available in my circuit).

 

Thanks in advance

 

Regards

Outcomes