AnsweredAssumed Answered

Need Quartus II "Project File(s)  [ NIOS II AD7980 project ]

Question asked by rmoshiri on Jun 28, 2012
Latest reply on Jun 29, 2012 by AdrianC

I successfully ran AD7980 Project on BeMicro NIOS II SDK. Can modify BeMicro SDK App in Eclipse development environment, download it to the device and run.

 

Now need to add a 2nd AD7980Eval Board, using the unused Cyclone IV pins that come through Transposer. Will wire them up to the 2nd AD7980Eval board.

 

Found a QUARTUS II Project file in the ADIEVALBoardLab directory. I am getting 3 errors (see below) and 41 warnings (see attached). Are there instructions for AD7980 project's QUARTUS II environment?

________________________________________________________________________________

Error (12006): Node instance "master_0_inst" instantiates undefined entity "master_0_master_0"

Error: Quartus II 32-bit Analysis & Synthesis was unsuccessful. 1 error, 41 warnings

    Error: Peak virtual memory: 280 megabytes

    Error: Processing ended: Thu Jun 28 17:39:17 2012

    Error: Elapsed time: 00:00:16

    Error: Total CPU time (on all processors): 00:00:15

Error (293001): Quartus II Full Compilation was unsuccessful. 3 errors, 41 warnings

Outcomes