AnsweredAssumed Answered

AD8488 and charge amplifiers in general

Question asked by AndyB on Jun 27, 2012
Latest reply on Jul 2, 2012 by jstaley

I'm working on an ion detector for a time-resolved mass spectrometer.  The detector will employ a simple Faraday cup.  Expected ion currents are in the range of 10 fA to 1 pA with a bandwidth of approximately 50 kHz.

 

The bandwidth makes this a difficult problem.  For DC or low bandwidth applications a high-gain transimpedance amplifier is typically used.  For our application a charge integrating amplifier is more appropriate.

 

The AD8488 has a charge amplifier front-end (well, 128 of them).  Its minimum feedback capacitance of 0.45 pF would give us the gain we need. Can the AD8488 be used as a single-channel charge integrator with a reset every 5 ms?

 

Besides the AD8488, are there amps which are appropriate to this application (e.g. FET input, very low input bias current, very low noise)?  Some off-the-shelf solutions (often called "charge sensitive preamplifiers") are hybrids that employ a discrete input FET (sometimes cooled).  Any suggestions in this regard would also be appreciated.

 

Thanks.

 

http://www.analog.com/en/specialty-amplifiers/charge-integrator-amplifiers/ad8488/products/product.html#

Outcomes