AnsweredAssumed Answered

BF527: NAND and Ethernet MAC usage simultaneously

Question asked by andreas.ru on Jun 28, 2012
Latest reply on Jun 29, 2012 by andreas.ru

We would like to develop a ucLinux based device on a BF527 that makes use of the internal MAC of BF527 and uses NAND flash for code storage. But from the documentation of EZ-Kit of BF527 I learned that MAC and NAND could not be used at  the same time on BF527. Is that really true?

 

What is the maximum size of external NOR Flash that I can use with BF527? Is it 4MByte?

 

Does anybody have a recommendation where to store the linux system? NOR flash or SPI flash?

Outcomes