AnsweredAssumed Answered

FIR filters with shift factors and abs(coefficents) > 32768

Question asked by goldscott on Jun 19, 2012
Latest reply on Jun 26, 2012 by goldscott

Hi All,

 

I primarily code FIR and IIR filters using the fir_fr16 and iir_fr16 library functions (all of my Blackfin code is in C). I'm coming from the golden era of ADSP-21xx assembly.

 

Two questions:

 

First question: I have an FIR filter where one of the coefficients is -36127. On the old 218x processor, I'd break the coefficient into two values (-18063 and -18064 in this case) and write a custom assembly function that would not increment the input data pointer until after the second multiply.

 

Is there a library function to handle coefficients greater than 32767 (or less than -32768)? Or am I going to have to modify the library function to handle this particular case? I'm not well-versed in Blackfin assembly.

 

--

 

Second question: This FIR filter also has an output scaling factor (in this case a multiply of 4 but will be coded as a left shift of 2). I'd like to round the accumulator and then perform the shift so as not to lose (in this case) 2 bits of precision. Is there a library function to handle this?

 

e.g. if we have an accumulator value of:

0x00 0123 AD72

 

we'd add 0x00 0000 2000 to round the LSB of our pre-shifted value, resulting in 0x00 0123 CD72

and then left shift 2, giving us our final 16-bit value in the high word, 0x00 048F 35C8

where we store 0x048F. This is obviously much better than simply shifting 0x0123 by 2, yielding 0x048C and losing precision.

 

Am I going to have to modify the library function to perform this arithmetic?

 

Any help, tips, advice would be appreciated.

 

Thanks,

Scott

Outcomes