AnsweredAssumed Answered

Clock Input Level of AD9517-3

Question asked by Kou on Jun 17, 2012
Latest reply on Jun 28, 2012 by pkern

Hello,

I am designing clock circuit using the AD9517-3.

I have two questions about CLK INPUTS.

 

Pls refer to P.6 Table3.

1.Data sheet describes "Input Level differential is 2Vp-p(Max).

Pls teach me the maximam input level of case of Single-Ended.

 

2.Also, "Larger voltage swings may turn on the protection diodes and may degrade jitter performance".

I think that it means Larger voltage swings may degrade jitter performance.

Could you explain me more detail?.
I'd like to know relation between input-level and jitter.

It would be greatly appreciated if advice could be gotten.

Best Regards,
Kou

Outcomes