AnsweredAssumed Answered

AD 9959 programming

Question asked by prince.beckham on Jun 8, 2012
Latest reply on May 15, 2018 by Tanzir

Hai

 

I got the evaluation board and its working fine, I can generate 300 kHz and 600 kHz signals.

(Single-bit serial mode (2-wire mode))

 

Now i wish to buy the 9959 chip alone and integrate it in my pcb, which pins are used for communication

which tools help me program the DDS?

I assume  SCLK, CS BAR, SDIO_0,SDIO_3  , PINS should be connected to USB port of computer?

can this pins be connected via mini B USB terminal to computer USB port?

does the same software which is used to control/program eval board is useful now?

 

please clarify

 

thanks and regards

Pratap

Outcomes