AnsweredAssumed Answered

ADA4932-1/2 use as Funnel Amplifier.

Question asked by Kou on Jun 5, 2012
Latest reply on Jun 5, 2012 by Kou

Hello,

I am designing differential ADC driver ciucuit,using ADA4932-1/2.

I'd like to design Funnel Amplifier.

Condition,below.

・Vin=±5V(span 10V),Single-end
・Vout_diff =2Vp-p,Gain-diff= x 0.2

 

The datasheet describes. below,
"Can be used with fractional differential gains"

Can I use ADA4932 as Funnel Amplifier?.

 

It would be greatly appreciated if advice could be gotten.

 

Best Regards,
Kou

Outcomes