AnsweredAssumed Answered

ADF4350 Evaluation board programming

Question asked by Yoh on May 31, 2012
Latest reply on Jun 4, 2012 by rbrennan

Hi,

 

I have an ADF4350 Evaluation board that I'm using in conjunction with the dlpll.cpp code as well as the the application software that comes with the evaluation board (I've tried two versions: Rev 2.5 2009 & Rev 4.0.3 March 2012). In all three cases I'm not able to tune the synthesizer faster than every 20ms. Is there another lower level program that I can use to be able to program a sequence of frequencies to tune to, much faster than every 20ms? Failing that is there a programmers guide available for the board that I can use to try and develop something?

 

Thanks

Yohannes

Outcomes