AnsweredAssumed Answered

AD9510 soft sync

Question asked by Malafaia on May 31, 2012
Latest reply on Jun 8, 2012 by pkern

Hi,

I'm having trouble with a 4DSP FMC108, 4adc at 250MHz implementation. It uses the AD9510 and I was having to much relative phase from the adc outputs. After I used softsync the relative phase became much lower. But sometimes the softsync doesnt seem to do anything, is my implementation wrong?

What I do is the following:

  - Read the soft sync register

  - Write the soft sync bit to '1'

  - Read the register till it got modified

  - Write the soft sync bit back to '0'

- Read the register till it got modified

  - Then proceed with the rest of the code

 

Best Regards,

  Daniel Malafaia

Outcomes