AnsweredAssumed Answered

Sweep mode in AD 9958.

Question asked by qpawelvn on May 29, 2012
Latest reply on Jun 22, 2012 by DSB

Hello. In LINEAR SWEEP MODE only works on a smaller (S0) function to a larger value (E0) ?

 

Here is my problem.

 

I need to continuously change the  frequency of the signal between the two values.

 

Option 1 - the initial value (S0) is less than the final (E0).

 

Option 2 - the initial value (S0) of more than a finite value (E0).

 

In the Option 1 of a sweep is running. In option 2 does not work (still on the starting value).

 

That's inherent in the architecture of chips or something I'm doing wrong?

 

 

 

Enclose two configuration file for the debug board  AD9959_ EVAL for option 1 and 2, respectively.

Attachments

Outcomes