AnsweredAssumed Answered

lower ADXRS620 output impedance , higher ADC accuracy ?

Question asked by Guillaume on May 23, 2012
Latest reply on Jun 6, 2012 by Harvey

Hi

I use LTC1408 (ADC) to convert ADXL325 and ADXRS620 analog signals. LTC1408 ask to use a buffer amplifier before ADC to transform the analog signals, which have high source impedance.

 

ADXL325 has an output impedance of 32k for LP filter, so it is necessary to add a buffer to the signal.

For ADXRS620, the temperature output impedance is very high, so it is also needed to put a unit buffer to the signal before ADC.

 

My question is where to know the impedance of the gyro's rate signal. Is it high or low? Is it essential to use a unit buffer to the signal if a high ADC accuracy is required?

 

Thanks in advance

Outcomes