AnsweredAssumed Answered

ADV7390 HD 720p  30Fps SDR

Question asked by aalqassis on May 22, 2012
Latest reply on Jul 12, 2012 by aalqassis

Hello,

 

I am currently working with ADV7390 (D/A) converter. In my project i am trying to convert a digital signal from an Omi Sensor (OV10630) to an analog signal using the expansion port for interface. The output format of the sensor is 8/10 bits YUV 4:2:2 720p at 30Fps SDR. I have been trying to set the register of the encoder to match the output format of the sensor but i was not able to get an image from the output of the encoder. I used the setting in table 118, however the setting is for 16 bit. But my input to the encoder is 10 bits. Would this work , if not how can i keep the same setting but change the input bit setting from 16 to 10 bit.

 

Thanks,

 

Adham

Outcomes