AnsweredAssumed Answered

ADAU1701 mono peak limiter with ext. detector

Question asked by Shahin on May 18, 2012
Latest reply on Aug 8, 2012 by BrettG

I'm working on a project in which I need mono peak limiters with an external detector but it appears that this feature is only available on the stereo peak detectors.

 

I'd like to add a couple more limiters but I'm just about out of memory.  I've used four stereo peak limiters with external detection and I'm running them all with mono signals.

 

If there was a mono version available, would that free up enough memory to add an additional two mono peak limiters w. ext. detection? If so, is there any way to get that block added to the library?

Outcomes