AnsweredAssumed Answered

8/16GB NAND Flash part suitable for BF52X series?

Question asked by G40 on May 17, 2012
Latest reply on May 24, 2012 by Prashant

We are trying to keep our core hardware design as close as possible to the BF526 EZBRD for sanity's sake. One problem is that our own hardware will have an 8 or 16GB Nand FLASH part connected to the BF52X NFC. Can anyone help with the following please?

 

1. Does the BF52X NFC actually support 64GBits MLC FLASH?

2. Does anyone have a part they would recommend. I understand Async mode, 8 bit data, is required, possibly ONFI compatible if from one of the ONFI consortium?

3. If the answer to 1 is yes, the question is then what, if any, driver changes are required? The model we are working from is based on the content from EE334.

 

Many thanks.

Outcomes