AnsweredAssumed Answered

Testing of Power Amplifier ADL5542 PCB

Question asked by neelmehta89 on May 15, 2012
Latest reply on May 15, 2012 by Jim

I have designed a ADL5542 (Power Amplifier) PCB as per the specifications in the datasheet. I want to test the performance and ensure that the PCB works fine before I link them up with other PCBs. So, can someone guide me as to what tests/equipment I can use to test this? Note that my emphasis is to check accuracy of the PCB rather than its performance.

 

Additional Info:

This PCB when linked to other PCBs form a communication circuit. This PCB is used as a power amplifier of signals below frequency of 1 GHz.

Outcomes