AnsweredAssumed Answered

Visual DSP Project Dependencies Issue

Question asked by ThomasR on May 11, 2012
Latest reply on May 15, 2012 by CraigG

Hi,

 

I'm using the BF561 DSK and try to get a minimal build together to boot my own code from the flash on the DSK. I started off using the power-on-self-test unchanged except for the generation of a loader file instead of a .dxe executable. Using the flash programmer VDSP API that worked fine.

Then I tried to remove the shared memory module for layer 2 and 3 and the project for core B. Unfortunately even after removing the dependencies from those three projects from the main BF561_EZKIT_POST project and updating the dependencies the build fails because the libraries sml2.dlb, sml3.dlb and coreB.dlb are still present in the .mak file.

Where in the IDE can I find the entries of those libraries?

 

Thank you very much,

Thomas

 

Win7/ Visual DSP 5.0.10.0/ EZ-KIT LITE BF561 Rev2.3

 

Message was edited by: Thomas R

Outcomes