AnsweredAssumed Answered

Wrong output from TMP05

Question asked by mrkozmic on May 9, 2012
Latest reply on May 10, 2012 by jtowey

Hi,

I have a TMP05 on my board configured in floating state (both CONV/IN and FUNC pins are not connected).

The TMP065 outputs a continous PWM signal as expected. The problem is that the high part of signal is 33ms on one board and 35ms on another and not 40ms as stated in the datasheet. Why is that?

 

The TMP05 is running at 3.3V.

 

Thanks in advance

Outcomes