AnsweredAssumed Answered

Need of help in design

Question asked by Karthikselvan on May 8, 2012
Latest reply on May 29, 2012 by Karthikselvan

Can anyone guide me suitable components for design a comb generator.

I need a stable 50 MHz clock frequency, and i have to divide that 50 MHz clock into 25 MHz, 5 MHz etc. Following that i need a 16:1 multiplexer which have to accept the above mentioned divided clocks and have to give any one of them based on selection line inputs.

On whole, i need

  1.   50 MHz clock,
  2.   a decade counter (as a frequency divider), have to divide 50MHz clock upto 4 (25MHz,5 MHz.... etc)
  3.   a 16:1 multiplexer.

Attachments

Outcomes